Max_Profile_Velocity
Max_Profile_Velocity
| Address: | 4117 (1015H) |
| Type: | DWORD |
| Access: | Read/Write |
| Unit: | Hertz |
| Range: |
(250*Motor_SPR / 65536) to (3276800*Motor_SPR / 65536) |
| Default Value: | 40000 |
| Store Supported: | Yes |
| Description: | It sets the maximum motor velocity for the acceleration and deceleration ramp. |
| Notes: |
This object can only be set with the motor at a standstill; this object must be higher than the Min_Profile_Velocity object. If the value to be set is lower than the minimum value range, the minimum value is stored. The Profile_Velocity object becomes equal to the value of the Max_Profile_Velocity object. |